Can USB-CAN Analyzer SKU 114991193 be programmed from C/C++ ?

Hi,



I’d like to know if it is possible to use the USB-CAN Analyzer to receive/send CAN frames from a C/C++ program developed in a PC.



If possible:

  1. What are the APIs, SDKs or libraries to be used?
  2. and what operating systems? Windows? Linux? Both?



    Thank you very much,



    Pablo

Hi,



You can find the docs related to Seeed USB-CAN Analyzer here

Hello,



Thanks for your reply, but in the documents you mention I can only see descriptions about how to use USBCAN software, not about developing/programming my own software using the USB-CAN Analyzer device.



We need to integrate some custom electronics boards (which include a CAN connection) to an existing software developed in my company, programmed in C++, in order to do that I am searching for a USB to CAN device which can be controlled (programmed) by ourselves, i.e. we need to add CAN communications to an existing software.



Best regards

We did manage to integrate this into a C# program but we’ve found that CAN baud rate change commands which worked with hardware V7.1 do not work with V8.0.

Is there different documentation available for V8.0?