Can the mic array be used as a way to locate the direction of nonvoice sounds?

There are two strange noises at my apartment. One is 1.5khz and the other is 6.5khz.

They are coming from outside my apartment and when I use rta with my umik1 it just doesn’t provide enough fidelity to hot/cold track the noises down.

I would like to try and use the microphone array to track them down. Any ideas if it can accomplish that goal?

I don’t think so, and I’m curious how you know the frequency of the noise.

I have a omnidirectional class 2 microphone.

I have the exact same need.
I have a (“birdy”?) noise in my yard at night and I would to track it down.

I registered a spetrum analysis with a android app and it showed a 1160 Hz signal.
I have just got a 4-Mic array respeaker with a raspberry.

I have launched the standard doa example (vad_doa.py in mic_array github repo).
But I would like to implement a new feature to filter given a frequency window around 1160 Hz.

Dude! I rented a CAE sound camera from The Moral Shop.

It was kind of expensive but one of the coolest things I have used!!