I need a help, I wanted to use rainbowduino to control high power LEDs (350mA on each channel), but with version 3 in Rainbowduino Wiki page, I can only drive 20.8 mA. Is this correct? If yes, why the previous version was discontinued?The only rainbowduino (I used to control the LEDs), burned
. Can you help me?
Dear customer,
Because version 3.0 control different LEDs so we need different parameters. And it is correct for 20mA.
If you want 2.0 board, sorry it is discontinued.