Hello!
I am not able to call my GPRS shield. It just hangs up. If I type AT then try again, it says the caller is not available at the moment.
I can make a call with it, a can send and receive message. But I can not call it. Why is that?
(Yesterday if I called the shield the monitor printed out “RING”). But now nothing. 
#include <SoftwareSerial.h>
SoftwareSerial mySerial(7, 8);
void setup()
{
mySerial.begin(19200); // the GPRS baud rate
Serial.begin(19200); // the GPRS baud rate
delay(500);
}
void loop()
{
if (mySerial.available())
Serial.write(mySerial.read());
if (Serial.available())
mySerial.write(Serial.read());
}
Thanks
Enjoy it.