It is not clear to me if I can use UartSBee and an XBee module to remotely program and run my Seeeduino board. Is this possible?If this is possible, what do I need to purchase and do? Thanks
Hi ,
Referring to the tutorial in the linkhttp://www.ladyada.net/make/xbee/arduino.html , i have managed to do this.
I used UartBee and Xbee S1 as transmitter, xbee shield and Seeeduino as receiver. After setting the xbee S1 according to the tutorial , i connect a 100nF capacitance from pin D3 on the receiver Xbee shield to reset of Seeeduino. And then , open the Arduino-1.0, and it work
Glad to share this if i have time.
Deray
Thank you for testing this out. Just to make sure I understand
the hardware path:
PC -> USB Cable -> UartSBee V4 -> XBee S1 RF -> transmit
receive -> XBee S1 RF -> XBee Shield -> Seeeduino
with D3 connected to Seeeduino reset.
Is this correct?
yes , but you should connect a 100nF capacitor from RTS to Seeeduino reset.
Oh, i miss somethings. As to Xbee Shieldhttp://www.seeedstudio.com/depot/xbee-shield-p-419.html?cPath=132_134 ,firstly, it is necessary to remove the R1 and add a solder bridge. Secondly, you should solder in a tiny jumper between the RTS pin and D3.
Deray