Can i use the lipo Rider pro like an UPS ?

Hello,

My question is in the title : Can i use the lipo Rider pro like an UPS ?

I want to use my raspberry Pi, and if the 220 volt is stopped, switch automatically on the battery but without reboot.
My raspberry need to work 24/24 7/7 what type of battery can i use for a SAFE installation.

thank for your help.

Same question here: Is it possible to use lipo rider pro as a UPS, keeping the usb connected to a wall adapter, and prevent the lipo to be used/drained as long as the wall adapter delivers power?