varlux
                
              
                
              
                  
                  
              1
              
             
            
              Hello everyone. In CAN-BUS Shield wiki page I read:
“With an OBD-II converter cable added on and the OBD-II library imported, you are ready to build an onboard diagnostic device or data logger.”
Ok…I have the cable and the shield, but where is the OBD-II library?
Thanks
Andrea
             
            
              
              
              
            
           
          
            
              
                loovee
                
              
              
                  
                  
              2
              
             
            
              Hi, I am sorry there’s no obd library, but a simple demo, please refer to github.com/Seeed-Studio/CANBUS_ … BD_RECIPLE
Thanks.
             
            
              
              
              
            
           
          
            
            
              Check out this:
https://www.libelium.com/api/waspmote/df/d8b/WaspCAN_8h_source.html
This is the only library I have found. It is limited though. I would like to start working on this, but I’m not sure if there is the demand for it.