CAN-Bus Shield and Mega 2560?

Hi ,
Actually , the Can-Bus Shield is using D10 - D13 pin as SPI port , but they are not connect to SPI pin , so if you want to use it with mega , you need to jump D10 - D13 to SPI pin . That is also a defect of this shield i think , i will give this info to the designer .

Regards,
Deray