Hi,
I’m heavily using Cory J. Fowler library
https://github.com/coryjfowler/MCP_CAN_lib
in many of my projects.
Today I need to set up speed of 50 kbps with no success.
Everything above 50 kbps works like a charm but below 100 kbps nothing works, neither sending nor receiving.
I’m trying to make 2 devices to talk to each other, my other CAN modules (not Arduino) work and communicate with each other @ 50, 20, 10 kbps etc. but not the Arduino one. I have updated the library to recent one but still no luck.
Any ideas? I tried with and without termination, wires are only 20 cm long.
Thanks for help
change it in the code to 50k set up in the code.