Calibration not working for me

Hi,

I’ve reformated the disk and after powering on I get the message “Parameter record not found”. - That’s ok, because there can’t be any.

I’ve again redone the whole calibration process for Ch-A as described above, but the values are again wrong.

DC Input to CH-A: 2,61V Quad says: Vpp: 3.12V, Vdc: 2.96V
DC Input to CH-A: 7.00V Quad says: Vpp: 7.52V, Vdc: 7.36V
DC Input to CH-A: 10.00V Quad says: Vpp: 11.0V, Vdc: 11.0V
DC Input to CH-A: 15.00V Quad says: Vpp: 14.3V, Vdc: 15.2V

If I power on and off the Quad, it says “reloading Parameter from disk”, but it doesn’t affect my voltage, it’s always wrong.

Edit: Just found out, that the Voltage is most off if I measure in the DC 5V Range. If I chang it to DC 2V the voltage is much more correct as in 5V!?