Is there a .net library for the SPI interface in Win10
Or do i need to use Linux to directly access SPI.
Is the bandwidth available over SPI similar to Raspbi Pi.
Is there a .net library for the SPI interface in Win10
Or do i need to use Linux to directly access SPI.
Is the bandwidth available over SPI similar to Raspbi Pi.
Recommend to use Linux to access SPI
Is there a mono library for Linux to access SPI or C or do i have to use Python ( yuck! )
Python also calls C.As long as you can see the /dev/spidev device, you can read and write through C in Linux.