Hi there,
So I ran this past my rep’s engineer and confirmed it with the AI,
the general consensus is The "LOGGING is Notorious for faults , check the forum…as well.
But You’re likely seeing a debug+logging-induced timing/stack issue, not flaky HW. Several things in that prj.conf can push Zephyr over the edge on nRF54L15—especially CONFIG_LOG_MODE_IMMEDIATE=y, high log level, and small/default stacks. Immediate logging runs in the caller’s context (often ISR), which is notorious for tripping faults on Nordic targets when combined with heavy debug builds. Zephyr Project Documentation+2Nordic Semiconductor Docs+2
What I’d try (in this order)
- Go deferred logging
CONFIG_LOG=yCONFIG_LOG_MODE_IMMEDIATE=nCONFIG_LOG_PROCESS_THREAD=yCONFIG_LOG_PROCESS_THREAD_SLEEP_MS=10- Drop the global level to INFO while testing:
CONFIG_LOG_DEFAULT_LEVEL=3
Rationale: avoids ISR-context logging + reduces pressure. Zephyr Project Documentation
- Bump stacks (debug builds use more stack)
CONFIG_MAIN_STACK_SIZE=2048CONFIG_ISR_STACK_SIZE=2048CONFIG_IDLE_STACK_SIZE=512- Keep:
CONFIG_STACK_SENTINEL=y(or yourCONFIG_MPU_STACK_GUARD=y, but note alignment/size constraints and that guard can fault sooner with tight stacks). Zephyr Project Documentation
- Trim “heavy” debug toggles
- Temporarily disable:
CONFIG_DEBUG_THREAD_INFO,CONFIG_DEBUG_OPTIMIZATIONS, maybe evenCONFIG_ASSERTjust to confirm sensitivity—then re-enable one by one.
- Console backend sanity
- If you’re using RTT:
CONFIG_USE_SEGGER_RTT=y,CONFIG_LOG_BACKEND_RTT=y. - If UART: keep RTT off to avoid two backends fighting.
- Re-test on NCS 3.1.1
3.1.1 does fix a handful of 3.1.0 paper cuts; several folks report better stability on 3.1.1 with the Xiao/54L15. (Your forum thread lines up with that trajectory.) Seeed Studio Forum - If still flaky, A/B the guard
- Try without
CONFIG_MPU_STACK_GUARDto see if it’s just catching undersized stacks (then restore it after tuning). Guarded stacks on Cortex-M require stricter alignment/size and can surface marginal configs as “bus faults.” Zephyr Project Documentation
Why I think it’s this
- The user can reproduce only with DEBUG enabled, and even Blinky trips it. That screams context/timing/stack rather than GPIO.
- Immediate logging in ISR context has a track record of crashes on Nordic targets when debug is on and stacks are tight.
Try something along these lines…
# Core
CONFIG_GPIO=y
# Logging (deferred)
CONFIG_LOG=y
CONFIG_LOG_DEFAULT_LEVEL=3
CONFIG_LOG_MODE_IMMEDIATE=n
CONFIG_LOG_PROCESS_THREAD=y
CONFIG_LOG_PROCESS_THREAD_SLEEP_MS=10
CONFIG_LOG_BACKEND_RTT=y
CONFIG_USE_SEGGER_RTT=y
# Debug (start light)
# CONFIG_ASSERT=y
# CONFIG_DEBUG=y
# CONFIG_DEBUG_INFO=y
# CONFIG_DEBUG_OPTIMIZATIONS=y
# CONFIG_DEBUG_THREAD_INFO=y
# CONFIG_THREAD_NAME=y
# Stacks
CONFIG_MAIN_STACK_SIZE=2048
CONFIG_ISR_STACK_SIZE=2048
CONFIG_IDLE_STACK_SIZE=512
CONFIG_STACK_SENTINEL=y
# Or: CONFIG_MPU_STACK_GUARD=y (swap in after stack sizes are proven)
If you want a smoking gun
Enable the fault dump and read CFSR/BFAR to confirm a BusFault from log/ISR pressure, then re-enable pieces until it returns. (Standard Cortex-M33 fault doc here.) Arm Developer+1
One more practical check
Make sure the Seeed Xiao nRF54L15 board files you use match your NCS version; stale board defs against 3.1.x can cause oddities. Folks on the Seeed forum reported better luck moving from 3.0.x→3.1.1 with the Xiao. Seeed Studio Forum
Bottom line: flip to deferred logging, grow stacks, dial back debug flags, and try 3.1.1. That combo should stop the bus faults on the Xiao 54L15.
HTH
GL
PJ ![]()