I erased the default OS from the internal memory of the EdgeBox RPi200. This model does not have an SD slot, so I burned the OS onto a USB, changed the device’s boot settings, and attempted to copy the OS to the eMMC. However, it didn’t work because the device boots up, but to get a display, I need to connect the USB. I need the system to run directly from the device without using the USB. Any help?
Hi there, and Welcome here,
I saw a post a while back about this or something similar ?? Did you check the Config menu on the RPi ? Did you try to disconnect USB or turn off Boot from USB after ? Something about the HDMI or DP not getting drivers because the USB is in there…YMMV
Also what commands did you use to transfer the system?
HTH
GL
PJ v: