Build Vision AI with reCamera!

Ready to work with reCamera? Walk through the whole pipeline to discover how reCamera, the tiny yet powerful AI camera, simplifies vision AI development:

  • Modular hardware layers: Customize to fit your needs
  • YOLO11 models native support: Run object detection and counting directly on-device with the Node-RED dashboard, or upload your own model
  • Expand possibilities: Access versatile vision AI applications from the SenseCraft AI model zoo to adapt to different scenarios

I really want that freekin gimbal!

Hi there,

Preaching to the choir here…
I have been watching the Git , no 3D prints Yet? So
Standing By… LOL

That STR-400 arm is Sweet at about 6K… :money_mouth_face:

1 Like

:police_car_light: FLASH SALE ALERT — Only 40 Hours Left! :police_car_light:
The reCamera Gimbal is now 50% OFF for a limited time!
:money_bag: $168 → $84
Perfect for AI vision, robotics, and edge AI projects:
:high_voltage: Double Brushless Motor
:high_voltage: CAN Interface
:high_voltage: 1 TOPS AI Performance
:high_voltage: Node-RED Support
:high_voltage: YOLO Model Pre-installed
:high_voltage: Fast Training & Deployment
:hourglass_not_done: The deal ends in 40 hours — once it’s gone, it’s gone.
:backhand_index_pointing_right: Grab yours now:

Half off…
:grin:

HTH
GL :slight_smile: PJ :v:

NOTE:
If you’re a hobbyist a parent or someone who wants to dip their toe into the AI this is the perfect device not only will it cover robotics but also some AI using the yolo models some other communications methods like CAN bus and some other cool interfaces

I’m guessing it is gone. Looks interesting. Wow, lots of limitations for new users. I have to wait 2 minutes between posts. So here I am typing away, killing time.

Hi there,

I did manage to snag one b4
:grin:

I have all the Parts to Build a LARGER ONE :mechanical_arm:
except the CAN-BUS camera board, so this will push that finally.

GL :slight_smile: PJ :v:

1 Like