Baozhu
13
@harris.shallcross
void U_TxC(char c){
huart2.Instance->TDR = (char)c;
while(!__HAL_UART_GET_FLAG(&huart2, UART_FLAG_TC));
}
void U_TxS(const char *s, uint8_t null){
HAL_GPIO_WritePin(BL_WKP_GPIO_Port, BL_WKP_Pin, 0);
HAL_Delay(2);
while(*s){
U_TxC(*s);
s++;
}
if(null) U_TxC('\0');
HAL_GPIO_WritePin(BL_WKP_GPIO_Port, BL_WKP_Pin, 1);
}
void U_TxSL(const char *s, uint8_t l){
while(l--){
U_TxC(*s);
s++;
}
}
#define BL_BUFLEN 256
volatile char ubuf[BL_BUFLEN] = {0};
volatile uint8_t newbldata = 0;
volatile uint16_t cc = 0;
void UART_Handler(void){
char c;
if(__HAL_UART_GET_FLAG(&huart2, UART_FLAG_RXNE)){
c = (char)huart2.Instance->RDR;
if(cc<BL_BUFLEN){
ubuf[cc++] = c;
}
if(c=='\0'){
newbldata = 1;
cc = 0;
}
}
}
/* USER CODE END 0 */
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_ADC_Init();
MX_TIM21_Init();
MX_USART2_UART_Init();
/* USER CODE BEGIN 2 */
//Wakeup bluetooth module
HAL_GPIO_WritePin(BL_PDN_GPIO_Port, BL_PDN_Pin, 1);
HAL_Delay(1);
HAL_GPIO_WritePin(BL_PDN_GPIO_Port, BL_PDN_Pin, 0);
HAL_Delay(1);
__HAL_UART_ENABLE_IT(&huart2, UART_IT_RXNE);
__HAL_UART_ENABLE(&huart2);
newbldata = 0;
U_TxS("TTM:NAM-?\r\n", 1);
while(!newbldata);
newbldata = 0; //Breakpoint to check for received name
uint8_t isconnect = 0, n=0;
/* USER CODE END 2 */
U_TxS("TTM:CIT-30ms\r\n", 1);
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
if(newbldata){
if(strstr(ubuf, "TTM:CONNECT") != NULL){
isconnect = 1; //Successfully connected
}
else if(strstr(ubuf, "TTM:DISCONNECT") != NULL){
isconnect = 0; //Successfully disconnected
}
else{
n++;
}
newbldata = 0;
}
//When connected, send string every second
if(isconnect){
HAL_Delay(1000);
U_TxS("hi\r\n",1);
}
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}