What is the maximum output current,the description says " continuously output large current to drive the brushless motor.
The motor that comes with the kit is 42blf01 and specifications are peack current amp 4.6A output power watts 26. But I need to now the maximum current and power that the kit can handle, to be able to select other motors
Hi @MFF, which Motor Shield you are using?