Brick and Grove RFID Reader - Compatibility & Connector

Dear Collegues,

I am working with the Electronic Brick 125 Khz RFID Card Reader, and I plan to change it for the Grove - 125Khz RFID Reader because right now there is not the stock I need to purchase for the first model, that I already tested. I have 2 questions:

  1. Can I replace Brick model with the Grove model, and everything will be the same ?
  2. What is the pitch for the 4 pin connector in this new Grove version ? Any connector suggestion ?

Thanks in advance for your help.

Pablo Cardona.
Cali - Colombia.

hi, the brick version and the grove version of this module are all the same ,just different on the connector. the brick version is 2.54 pin, and the Grove is 2.0 .
thanks.