Hello somebody knows if the bluetooth in Xadow GSM+BLE is supported in IOS because I tested the BTserver example but only in Android is visible, so is posible connect to IOS?.
“For iOS, ANCS protocol is supported”
Source: LinkIt Assist 2502 Developer’s Guide, section 5.19
Also the “for more information” links to this: labs.mediatek.com/fileMedia/down … 4df8425a4d