Hello - i’ve been tinkering with the bluetooth shield off and on for a week or so now…
I am attempting to use it as part of a 3 person, engineering design 2 (senior class) for my computer engineering degree program…
I’m having issues connecting to the bluetooth module : I am running the module as the master, and attempting to connect to it with my HTC Evo 4G.
The shield will recognize my phone, based off the set name, and address…it will pop up the dialog box on my phone asking to input the pin…but every time I input the pin (0000, 1234) it just returns a connection failure…
I’ve been through the wiki multiple times and googled around but cannot for the life of me get the two devices to just connect and pair properly…
Any sort of help or guidance will be super appreciated…