Subject says it all: I use the demo code to setup the bluetooth shield as a slave. I have a linux PC with a BT dongle.
Connection is OK using gtkterm as serial terminal and the arduino serial term to the arduino.
If I send chars from the arduino serial term to the bluetooth shield, it is received in the gtkterm window (the one connected to /dev/rfcomm0), but not the other way around: if I type something in gtkterm it does not appear in the serial term window.
It’s like its only one-way comm!
The speeds are ok: 9600 for /dev/ttyUSB0 and 38400 for /dev/rfcomm0.
Any idea?
TIA
Hi there,
Can you provide your code ?
Deray
Hi,
firstly there is in fact 2-way communications, but from arduino to remote PC it is perfect (BTW I can use whatever baudrate on the remote PC and it works!), but the other way around, I only get mostly chars with 255 ascii codes, and also, it is not 1-1, that is I can try to send 10 chars and get only 4 or 5 chars. Moreover if I hold a key on the remote PC I get mostly 255-ascii coded chars but sometimes also 254, or others, but almost the higher 4bits are all set that is in hexa it is: Fx where x is different from time to time.
Here is the code (it is very similar to the example code):
#include <SoftwareSerial.h> //Software Serial Port
#define RxD 7
#define TxD 6
#define DEBUG_ENABLED 1
SoftwareSerial blueToothSerial(RxD,TxD);
void setup()
{
Serial.begin(9600);
pinMode(RxD, INPUT);
pinMode(TxD, OUTPUT);
setupBlueToothConnection();
}
void loop()
{
char recvChar;
while(1){
if(blueToothSerial.available()){//check if there's any data sent from the remote bluetooth shield
Serial.println("available!!");
recvChar = blueToothSerial.read();
Serial.print(recvChar);
blueToothSerial.print(recvChar);
}
if(Serial.available()){//check if there's any data sent from the local serial terminal, you can add the other applications here
recvChar = Serial.read();
blueToothSerial.print(recvChar);
}
}
}
void setupBlueToothConnection()
{
blueToothSerial.begin(38400); //Set BluetoothBee BaudRate to default baud rate 38400
blueToothSerial.print("\r\n+STWMOD=0\r\n"); //set the bluetooth work in slave mode
blueToothSerial.print("\r\n+STNA=SeeedBTSlave\r\n"); //set the bluetooth name as "SeeedBTSlave"
blueToothSerial.print("\r\n+STOAUT=1\r\n"); // Permit Paired device to connect me
blueToothSerial.print("\r\n+STAUTO=0\r\n"); // Auto-connection should be forbidden here
delay(2000); // This delay is required.
blueToothSerial.print("\r\n+INQ=1\r\n"); //make the slave bluetooth inquirable
Serial.println("The slave bluetooth is inquirable!");
delay(2000); // This delay is required.
blueToothSerial.flush();
}
Set all baudrates to 9600.
OK thanks will try that ASAP and report here.
OK it is fixed now but for another reason: I changed the RX pin to another one and now it works. It really is weird as I am pretty sure I tried with another board (an UNO actually) and it did not work. Anyway its probably my Duemilanove which is abit borked somehow.
Thanks.