I am new and could use some help getting my devices to connect to the Bluetooth shield board. I am able to get the BT Shield board into inquirable mode since the red and green lights are flashing. However when I try to connect my Windows Phone 8 device or Windows laptop to the BT Shield, it immediately shows up as connected and then disconnected and the red and green lights keep flashing. In addition, I can communicate fine with the device via sscomm sending it commands and getting the appropriate responses but a connection never happens via that method either. Any help would be appreciated to get me out of the Christmas light flashing mode and into the cool green connected mode
[code]/*
BluetoothShield Demo Code Slave.pde. This sketch could be used with
Master.pde to establish connection between two Arduino. It can also
be used for one slave bluetooth connected by the device(PC/Smart Phone)
with bluetooth function.
2011 Copyright © Seeed Technology Inc. All right reserved.
Author: Steve Chang
This demo code is free software; you can redistribute it and/or
modify it under the terms of the GNU Lesser General Public
License as published by the Free Software Foundation; either
version 2.1 of the License, or (at your option) any later version.
This library is distributed in the hope that it will be useful,
but WITHOUT ANY WARRANTY; without even the implied warranty of
MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU
Lesser General Public License for more details.
You should have received a copy of the GNU Lesser General Public
License along with this library; if not, write to the Free Software
Foundation, Inc., 51 Franklin St, Fifth Floor, Boston, MA 02110-1301 USA
For more details about the product please check http://www.seeedstudio.com/depot/
*/
/* Upload this sketch into Seeeduino and press reset*/
#include <SoftwareSerial.h> //Software Serial Port
#define RxD 2 // A loose pin required me to move my connection jumpers but it appears to still work since I can get command responses
#define TxD 3
#define DEBUG_ENABLED 1
SoftwareSerial blueToothSerial(RxD,TxD);
void setup()
{
Serial.begin(9600);
pinMode(RxD, INPUT);
pinMode(TxD, OUTPUT);
setupBlueToothConnection();
}
void loop()
{
char recvChar;
while(1)
{
if(blueToothSerial.available())
{//check if there’s any data sent from the remote bluetooth shield
recvChar = blueToothSerial.read();
Serial.print(recvChar);
}
if(Serial.available())
{//check if there’s any data sent from the local serial terminal, you can add the other applications here
recvChar = Serial.read();
blueToothSerial.print(recvChar);
}
}
}
void setupBlueToothConnection()
{
blueToothSerial.begin(38400); // Set BluetoothBee BaudRate to default baud rate 38400
blueToothSerial.print("\r\n+STWMOD=0\r\n"); // set the bluetooth work in slave mode
blueToothSerial.print("\r\n+STNA=SBS\r\n"); // set the bluetooth name as “SeeedBTSlave”
blueToothSerial.print("\r\n+STOAUT=1\r\n"); // Permit Paired device to connect me
blueToothSerial.print("\r\n+STAUTO=0\r\n"); // Auto-connection should be forbidden here
delay(2000); // This delay is required.
blueToothSerial.print("\r\n+INQ=1\r\n"); // make the slave bluetooth inquirable
Serial.println(“The slave bluetooth is inquirable!”);
delay(2000); // This delay is required.
blueToothSerial.flush();
}[/code]