Bluetooth bee +bees shield , it works?

Hi everybody, I’m trying to make work a bluetooth bee module on a bees shield with arduino UNO R3.
seeedstudio.com/depot/blueto … p-598.html
seeedstudio.com/depot/bees-shield-p-672.html
It’s seem not work to me.

I want to make a simple discovery of all nearby MAC address.

I put the jumper BEE_1 RX on PIN 5 and BEE_1 TX pin PIN 6

And the code that i use , is this:

#include <SoftwareSerial.h>   //Software Serial Port

#define RxD 5
#define TxD 6
 
#define DEBUG_ENABLED  1

char recvChar;
String recvBuf;
String recvAddr;
String recvInq;

SoftwareSerial blueToothSerial(RxD,TxD);
 
void setup() 
{ 
  Serial.begin(9600);
  pinMode(RxD, INPUT);
  pinMode(TxD, OUTPUT);
  setupBlueToothConnection();
  //wait 1 sec and flush the serial buffer
  delay(1000);
  Serial.flush();
  blueToothSerial.flush();
  Serial.println(" ");
  Serial.println("restarted....");
  Serial.println("Starting BTScan....");

} 

void loop()
{
  btScan();
}

void setupBlueToothConnection()
{
  blueToothSerial.begin(38400); //Set Bluetooth to 38400
  blueToothSerial.print("\r\n+STWMOD=1\r\n");//set bluetooth to master mode
  blueToothSerial.print("\r\n+STNA=MyBTname\r\n");//set bluetooth name 
  blueToothSerial.print("\r\n+STAUTO=0\r\n");// no Auto-connection
  delay(2000); // This delay is required.
  blueToothSerial.flush();
  blueToothSerial.print("\r\n+INQ=1\r\n");//make the master inquire
  delay(2000); // This delay is required.
}
    
void btScan()  //scan for devices
{
  if (blueToothSerial.available())
  {
    recvChar = blueToothSerial.read();
    recvBuf += recvChar;
    if (((recvChar > 47) && (recvChar < 58)) || ((recvChar > 64) && (recvChar < 71)))  // get numbers and A-F only
    {
      recvAddr += recvChar;
      if(recvAddr.length()==12)
      {
        Serial.println(recvAddr);
        recvAddr = "";
        blueToothSerial.flush();
      }
    }
  }
}

It’s seems correct, but the blueToothSerial does not seem turn available.

My question is:
If the code is correct, it is possible that the two components are not compatible?
What could be wrong?

Thanks in advance

hey , you need put the jumper BEE_1 RX on PIN 6 and BEE_1 TX pin on PIN 5.

Thank’s IT WORKS! :mrgreen: