Blob_boot0.imgimg Error on reComputer j4012

Hello,

I am experiencing an error while flashing JetPack 6.1 onto my Jetson Orin NX 16GB module, installed on a reComputer J401 carrier board. I initially tried using NVIDIA’s SDK Manager, but encountered issues and then followed the instructions in this document: Flash Jetpack | Seeed Studio Wiki

However, I am still encountering an error. The error message I am receiving is “Stat for blob_boot0.imgimg failed”.

Entering RCM boot

[ 0.0842 ] mb1_t234_prod_aligned_sigheader.bin.encrypt filename is from --mb1_bin
[ 0.0842 ] psc_bl1_t234_prod_aligned_sigheader.bin.encrypt filename is from --psc_bl1_bin
[ 0.0842 ] rcm boot with presigned binaries
[ 0.0891 ] tegrarcm_v2 --instance 2-1.2 --new_session --chip 0x23 0 --uid --download bct_br br_bct_BR.bct --download mb1 mb1_t234_prod_aligned_sigheader.bin.encrypt --download psc_bl1 psc_bl1_t234_prod_aligned_sigheader.bin.encrypt --download bct_mb1 mb1_bct_MB1_sigheader.bct.encrypt
[ 0.0899 ] BR_CID: 0x80012344705DF18C8C0000000E030180
[ 0.1265 ] Sending bct_br
[ 0.1480 ] Sending mb1
[ 0.1568 ] Sending psc_bl1
[ 0.1698 ] Sending bct_mb1
[ 0.1755 ] Generating blob for T23x
[ 0.1848 ] tegrahost_v2 --chip 0x23 0 --generateblob blob.xml blob.bin
[ 0.1857 ] Stat for blob_boot0.imgimg failed
Error: Return value 19
Command tegrahost_v2 --chip 0x23 0 --generateblob blob.xml blob.bin
Cleaning up…

Hi there,

So is that in the matrix on the WiKi for Jetson?
i.e j401 that is?
Can you give an overview what you did to flash? the SD or NVME , Linux host or Ubuntu host etc…
HTH
GL :slight_smile: PJ :v:

Here are the components of my system:

Hi there,

Excellent UNIT!. So I see this , is why I asked…
I used ubuntu 18.04 as host machine during the first installation and I encountered the error mentioned above. Then I switched to Ubuntu 20.04 and the installation ended successfully."

It appears the Tegra stuff is messing up the last file system check
Others faced it as well, G-man shows this thread short but good info.

Switch up your Ubuntu host or, look more into the downloads you may be have both files the original and the one for the NVIDIA on the system confusing it. YMMV

HTH
GL :slight_smile: PJ :v:

Thank you for your help and time. Using PJ_Glasso Ubuntu 20.04 solved my problem and the flash process was completed successfully. Best regards.

Hi there,
Awesome Glad you got it going, one because its’ a Rocket at 100 Flops so and NOT cheap either. I hope they all converge a little better on the future software & JP’s " it’s all Open source" :lying_face: LOL
so they say!

Post up some of your results on models and inferencing and such if possible. That local DeepSeek r1 stuff is really impressive. :+1:

GL :slight_smile: PJ :v: