BLE Advertising Current Comparison, ESP32C3,C6,S3, MG24, nRF52840

Any chance the nRF54L15 can have an additional flash to store programs? Like 4mb? my main reason to abandon the previous nRF52840 was because of the 1.5mb available memory. My project code is close to 2mb and then I still need the space for OTA updates. However, frankly speaking, the 2mb code is due to the BLEDevice ESP32 library, so in Nordic world that can be probably smaller?