BLE Advertising Current Comparison, ESP32C3,C6,S3, MG24, nRF52840

Hi there,

I’M with you on that for sure…
Let’s hope they get the next one totally right.
We sure do alert them to the pitfalls and short comings… so hopefully there all :ear: ears.

Seems the LDO’s. Give seeed engineers heartburn, lol​:grinning:, along with the “reading” battery soc… I’m hopful for a PMIC chip also I2C readable ,EVERYONE else in the the battery or wearable devices are implementing them. ABOUT TIME​:grin::+1:
The wio terminal has a MAX chip ,they should stick to the basics and make it happen.

GL :smiley: PJ :v: