Hi, new DSO 201 owner here trying to install the BenF firmware, unsuccessfully so far. It came with firmware 4.28.
In DFU mode, the screen reports:
NiN
digital storage oscilloscope
Serial: DDDAB8BB License: 41BE9A7F
Device Firmware Upgrade: V3.29D
Please copy Hex or Bin file to
the DFU virtual USB disk.
I copy the BENF_P2.hex file from BenF_3.64APP_3.53LIB_patched_v2.zip to the device and I see it deactivate and come back, with now BENF_P2.RDY on it. Power cycle the device, and I’m back to the 4.28 version. It seems like the device thinks it has installed the new firmware, but not actually.
I have tried various other firmware versions. Every now and then it works correctly. At the moment I’m on firmware v4.30, but I have not yet managed to get the BenF version to install. Any ideas? Google led me here, and has found plenty of discussion of firmware install failures, but none quite like this.
In messing around with the device, I found a hardware information screen. Power up with the [-] and [M] buttons held down and I get a screen that looks like:
NiN
digital storage oscilloscope
Hardware: Version 1.7B
MCU Type: STM32F103VB
LCM Ctrl: ILI_9341
USB Disk: Ext MSD Card
I haven’t seen this mentioned anywhere else, though it seems unlikely that I’d be the first to stumble upon it.