My BBGW seems to have the eMMC corrupted. The power and WLAN LEDs stay on, but the user leds isn’t blinking. In the device manager it’s possible to see that the beaglebone is beeing reconized, but it don’t start as USB card in “My Computer”. I tryed to boot by SD card and tryed to flash a new image to the eMMC, but nothing works. Is there something I can do?
*the same SD card was tested on a BBB and it works.
Hi,
You’ll need to follow the instructions at <LINK_TEXT text=“http://elinux.org/Beagleboard:BeagleBon … shing_eMMC”>http://elinux.org/Beagleboard:BeagleBoneBlack_Debian#Flashing_eMMC</LINK_TEXT> . When the flashing is complete, all 4 USRx LEDs will be steady on or off. The latest Debian flasher images automatically power down the board upon completion. This can take up to 45 minutes. Power-down your board, remove the SD card and apply power again to finish.
Src : https://beagleboard.org/getting-started
Thank you for the reply.
There is a problem, the beaglebone don’t boot with the SD card. I also did a test with the serial communication, and the display only shows “CCCCCC”.
Hi,
what the problem while you are trying to boot with the SD card ? can you please share more detail?
The power and bluetooth LEDs stay on, but the user leds don’t blink. The system don’t boot with SD card. It’s stay the same without the SD card. When I try the same SD card in a Beaglebone Black, it boot normaly.