I have both a BBG and a BBGG. I’ve downloaded and flashed this image onto my 16gb microSD card:
- bone-eMMC-flasher-debian-10.10-iot-armhf-2021-10-01-4gb.img.xz
 
On my BBG I’ve successfully booted off this image on the SD card and flashed the eMMC flash. Removing the sd card afterwards confirms.
However, using the same sd card on my BBGG I cannot get it to boot off the sd card to start flashing the eMMC. At least I don’t think it’s working because I don’t see much activity on the sd card LED and I don’t see it get into the “back and forth” LED mode while flashing.
Is there something special I need to do to get my BBGG to boot off the sd card?
Should I be using a different image to flash onto the sd card?
Thank you