BBG not recognising a particular USB device

I need to connect my BBG to a solar inverter via USB. With a Linux or Windows PC the inverter is plug und play. However the BBG does not want to talk to it. Here is dmesg ourput:

[  313.129463] musb-hdrc musb-hdrc.1: Babble
[  313.231501] usb usb1-port1: attempt power cycle
[  314.779614] usb 1-1: new low-speed USB device number 31 using musb-hdrc
[  315.003650] musb-hdrc musb-hdrc.1: Babble
[  315.007743] musb-hdrc musb-hdrc.1: Babble
[  315.902757] musb-hdrc musb-hdrc.1: Babble
[  315.906865] musb-hdrc musb-hdrc.1: Babble
[  316.222830] musb-hdrc musb-hdrc.1: Babble
[  316.226935] musb-hdrc musb-hdrc.1: Babble
[  316.721876] musb-hdrc musb-hdrc.1: Babble
[  316.725984] musb-hdrc musb-hdrc.1: Babble
[  317.204063] usb usb1-port1: Cannot enable. Maybe the USB cable is bad?
[  317.281971] musb-hdrc musb-hdrc.1: Babble
[  317.286073] musb-hdrc musb-hdrc.1: Babble
[  317.335959] usb 1-1: new low-speed USB device number 32 using musb-hdrc
[  318.381080] musb-hdrc musb-hdrc.1: Babble
[  318.385180] musb-hdrc musb-hdrc.1: Babble
[  318.440119] usb 1-1: new low-speed USB device number 33 using musb-hdrc
[  319.360203] musb-hdrc musb-hdrc.1: Babble
[  319.364307] musb-hdrc musb-hdrc.1: Babble
[  319.820257] musb-hdrc musb-hdrc.1: Babble
[  319.824411] musb-hdrc musb-hdrc.1: Babble
[  320.807024] usb 1-1: New USB device found, idVendor=0665, idProduct=5161, bcdDevice= 0.02
[  320.807045] usb 1-1: New USB device strings: Mfr=3, Product=1, SerialNumber=0
[  320.825392] hid-generic 0003:0665:5161.0034: hiddev0,hidraw0: USB HID v1.11 Device [HID 0665:5161] on usb-musb-hdrc.1-1/input0
[  320.879391] musb-hdrc musb-hdrc.1: Babble
[  320.883603] musb-hdrc musb-hdrc.1: Babble
[  320.897304] usb 1-1: USB disconnect, device number 33
[  322.232576] usb 1-1: new low-speed USB device number 34 using musb-hdrc

The goal is to redirect the USB port across the LAN to my laptop. Tested and working under Linux Mint. Here is dmesg from Mint:

[ 52.422323] usb 2-4: new low-speed USB device number 2 using ohci-pci
[ 52.743386] usb 2-4: New USB device found, idVendor=0665, idProduct=5161, bcdDevice= 0.02
[ 52.743389] usb 2-4: New USB device strings: Mfr=3, Product=1, SerialNumber=0
[ 54.244930] hidraw: raw HID events driver © Jiri Kosina
[ 54.535652] usbcore: registered new interface driver usbhid
[ 54.535654] usbhid: USB HID core driver
[ 54.688050] hid-generic 0003:0665:5161.0001: hiddev0,hidraw0: USB HID v1.11 Device [HID 0665:5161] on usb-0000:00:02.0-4/input0

Using latest Debian 10 IoT image. Redirecting the port with a USB stick works fine using Virtualhere.

Is there any way to ‘teach’ Debian on the BBG how to talk to this device?

Thanks in advance,
Peter.

This should be fine if you use a mirror image of beaglebone

You mean another type of distro?

Thank you, @Baozhu, I loaded Ubuntu and it works now.