The current CE Certificate of Conformity for the BBG in part rests on testing done to show compliance with the EN55022 standard. The problem is that this standard is outdated and no longer accepted everywhere. (It is superseeded by EN55032.)
Does anybody know if more recent testing was done (e.g. with the 2016 BBG revision), and if the corresponding test reports are available? Without these the BBG can’t really be used in any commercial application without causing compliance problems.
Any help appreciated!