Manual says 3V button battery. CR2032 doesn’t fit… does anyone know the battery number?
Thanks.
Hi ashtown1
the battery number is CR1220.
Best regards
fy
This information is still not included in the online docs Grove - GPS (Air530) | Seeed Studio Wiki
Hi there,
So on the post for the "Air530 GPS " with ESPc3 & Nrf52840 I used both with the Dev Expansion Board Powered with a Square and Round 350Mah and a 450Mah (3.85Vdc) Lipo’s and they each worked GREAT! You can use the DigiKey On-Line Battery life calculator if you know YOUR circuits current consumption and Size accordingly.
Check out that thread on here… ![]()
HTH
GL
PJ ![]()