Hi, thanks for your reply. I have already tried but it’s not working. Not sure if I’m doing things right though. Here’s what I did:
xrandr
Screen 0: minimum 8 x 8, current 1920 x 1080, maximum 32767 x 32767
DP-0 disconnected (normal left inverted right x axis y axis)
DP-1 connected primary 1920x1080+0+0 (normal left inverted right x axis y axis) 800mm x 330mm
1920x1080 60.00*+ 59.94 50.00
1680x1050 59.95
1600x1200 60.00
1280x1024 75.02 60.02
1280x800 59.81
1280x720 59.94 50.00
1152x864 75.00
1024x768 75.03 60.00
800x600 75.00 60.32
720x576 50.00
720x480 59.94
640x480 75.00 59.94 59.93
cvt 3440 1440 60
# 3440x1440 59.94 Hz (CVT) hsync: 89.48 kHz; pclk: 419.50 MHz
Modeline "3440x1440_60.00" 419.50 3440 3696 4064 4688 1440 1443 1453 1493 -hsync +vsync
xrandr --newmode “3440x1440_60.00” 419.50 3440 3696 4064 4688 1440 1443 1453 1493 -hsync +vsync
xrandr --addmode DP-1 “3440x1440_60.00”
X Error of failed request: BadMatch (invalid parameter attributes)
Major opcode of failed request: 140 (RANDR)
Minor opcode of failed request: 18 (RRAddOutputMode)
Serial number of failed request: 25
Current serial number in output stream: 26
For reference, under Jetpack 5.1.2, xrandr only shows HDMI-0 with correct resolutions detected. Not sure how HDMI-0 became DP-0 and DP-1 under Jetpack 6.
Thanks!