I am trying to setup my A603 carrier board with my Jetson Orin NX 8GB module. I have flashed my system with Jetpack 6.0 as per the instructions given on: A603 Carrier Board | Seeed Studio Wiki
When I connect my screen to the hdmi port, the maximum resolution I can select is 1920x1080.
I have also tried flashing Jetpack 5.1.2 and it works perfectly, higher resolutions are being detected for my screen. Unfortunately I need Ubuntu 22.
I am happy to provide command outputs or any other information that might be helpful.
X Error of failed request: BadMatch (invalid parameter attributes)
Major opcode of failed request: 140 (RANDR)
Minor opcode of failed request: 18 (RRAddOutputMode)
Serial number of failed request: 25
Current serial number in output stream: 26
For reference, under Jetpack 5.1.2, xrandr only shows HDMI-0 with correct resolutions detected. Not sure how HDMI-0 became DP-0 and DP-1 under Jetpack 6.