Hello all. I recently purchased two of the Seeed XBee Shield V2.0 shields and i had a couple of queries:
- On the the wiki page there is no demo code for the shields, can the Software serial code be used?
- Is the maximum current supplied by the on-board 3.3v regulator more than 200ma to use with the xbee pros?
My hardware is
Robot:
-4WD controlled with 4 speed controllers (using servo library)
Transmitter:
-Arduino Uno (will be replaced with Leonardo for more analog inputs)
-1602LCD Display for telemetry
-Xbee series 1 1mw. (will upgrade to series 1 pro)
Receiver:
Arduino Mega 2560
-Xbee series 1 1mw. (will upgrade to series 1 pro)
-temp sensors, light sensor, sd card module (not shield), real time clock
Thank you! If there will be any more advice that anyone can provide that will be just great!