Arduino

Hi! Wunderhorn1, thanks for your info. The IR remote i referring to is
315Mhz remote relay switch kits - 2 channels i guess this is good enough cause 2 channels for 2 motor… just nice. right?

For the full-size gate motor specification is as follow:
Motor voltage supply 24V~
Motor power 100W
Thrust force (max.) 1200N
So, i just need to do some modification to suit Arduino main board…

Anyone who have any comment just drop in your post… :slight_smile: