Arduino Studio 1.6.3 with Xadow?

i have tried it with the new 1.6.4 (make a fresh install, add the files from github) and then i load the UserLed example.
now i get this:

Sorry, now it works.
I had not noticed two things.

  1. To utilize the version 1.6.x should I only the two files for 1.6.3 are not using the other.
  2. I have to adjust not only the Board (in my case Xadow) but also the programmer to “USBtinyISP”.