Arduino MKR Connector Carrier (Grove Compatible) + (MKR1000/MKR1010) with Grove Temp & Humid (DHT11) - Compatible..?

hello everyone,



a pleasant day to you!



i bought the following:

• 1 Seeed Grove temperature & Humidity (DHT11) sensor

• 2 Arduino MKR Connector Carrier (Grove Compatible)



to have a prototype for MKR1000 and MKR1010



when i put it all together

  1. MKR-Connector-Carrier + MKR1000 + Grove DHT11
  2. MKR-Connector-Carrier + MKR1010 + Grove DHT11



    • installed Library on my IDE: Grove Temperature And Humidity Sensor by Seeed Studio Version 1.0.0

    • Get the sample sketch DHTtester and modify DHTTYPE to DHT11
    [code]// Example testing sketch for various DHT humidity/temperature sensors
    // Written by ladyada, public domain

#include “DHT.h”
#define DHTPIN A0 // what pin we’re connected to

#define DHTTYPE DHT11 // DHT 11
//#define DHTTYPE DHT22 // DHT 22 (AM2302)
//#define DHTTYPE DHT21 // DHT 21 (AM2301)

DHT dht(DHTPIN, DHTTYPE);[/code]

• Uploaded sample sketch (DHTtester) to MKR board





The result are below:


  1. by the way, i tested Grove-DHT11 on UNO with Seeed Base-Shield and it works excellent!

  1. however, on MKR1000

  1. and on MKR1010


seems it satisfy both conditions (detecting NaN and with value afterwards during loop) but zero value
<CODE><s>[code]</s>// check if returns are valid, if they are NaN (not a number) then something went wrong!
if (isnan(t) || isnan(h)) 
{
    Serial.println("Failed to read from DHT");
} 
else 
{
    Serial.print("Humidity: "); 
    Serial.print(h);
    Serial.print(" %\t");
    Serial.print("Temperature: "); 
    Serial.print(t);
    Serial.println(" *C");
}<e>[/code]</e></CODE>

please kindly help me with my project,
i can't find any documentation regarding these items,
i worry now if these parts are compatible with each other...

thank you so much..

Hi there,

It is compatible. please refer to <LINK_TEXT text=“https://www.hackster.io/doncoleman/mkr1 … sor-8f22ed”>https://www.hackster.io/doncoleman/mkr1000-temp-and-humidity-sensor-8f22ed</LINK_TEXT> and <LINK_TEXT text=“https://www.pubnub.com/blog/2016-06-29- … o-mkr1000/”>https://www.pubnub.com/blog/2016-06-29-wirelessly-tracking-temperature-data-with-the-arduino-mkr1000/</LINK_TEXT> as well. thanks.