I cannot connect with bluetooth My ArduinoMega 2560 ADK . I have try method describe for Arduino Mega but cannot connect shiled with any device
Amigadroid
I cannot connect with bluetooth My ArduinoMega 2560 ADK . I have try method describe for Arduino Mega but cannot connect shiled with any device
Amigadroid
Dear customer,
I’m not sure what problem with you connecting?
Is it not pair with or others? What device do you want to connect with? It is use in Bluetooth 2.0?
Did you set the mode?
So please provide more information here it could be helpful.
Best regards,
Yuri
I can paired my devoce , but cannot make connexion with the Arduino bluetooth
I have try with Window 7 , Android 2,3 ( Galaxy note ) , Android 3.2 ( Acer Iconia A500) and Android 4 Asus transformer
Yes i use bluetooth 2.0
amigadroid
I can paired my devoce , but cannot make connexion with the Arduino bluetooth
I have try with Window 7 , Android 2,3 ( Galaxy note ) , Android 3.2 ( Acer Iconia A500) and Android 4 Asus transformer
Yes i use bluetooth 2.0
amigadroid
Dear customer,
You can pair your Bluetooth seem it is work correctly.
So if you download our Arduino 1.0 libraries from our WIKI. There is a TXT to remind you if you use MEGA2560 you should change to other pins with jumper wire.
Note:For SoftwareSerial to be able to receive serial data somewhat asynchronously, a receive pin needs to be able to trigger an external interrupt.So pin2…pin7 on Mega board should not be defined as sofeware serial port.
And it is only the following can be used for RX: 10, 11, 12, 13, 50, 51, 52, 53, 62, 63, 64, 65, 66, 67, 68, 69 pin.
So you need to jump by some wire with the board.
On the WIKI there is a photo show you where you should plug the jumper wire.
Best regards,
Yuri