Hello,
I get only 8 bytes from response of VIN Code request:
Do you know what is the problem?
Thank you.
Hello,
I get only 8 bytes from response of VIN Code request:
Do you know what is the problem?
Thank you.
Any idea of my problem?
Hello,which particular product are you using? Is it the Can-Bus shield V2 or CANBed? Please post with the link.
Hi There ,
What happens if you uncomment those first to line of code out.
//Serial.println(len, HEX);
//unsigned char buf[8];
void taskCanRecv() {
unsigned char len = 0;
//Serial.println(len, HEX);
//unsigned char buf[8];
while (CAN_MSGAVAIL == CAN.checkReceive()) { // check if get data
CAN.readMsgBuf(&len, buf1); // read data, len: data length, buf: data buf
Serial.println("\r\n------------------------------------------------------------------");
Serial.print("Get Data From id: 0x");
Serial.println(CAN.getCanId(), HEX);
//Serial.println(len, HEX);
for (int i = 0; i < len; i++) { // print the data
Serial.print("0x");
if(buf1[i] < 0x10) // If data byte is less than 0x10, add a leading zero
{
Serial.print("0");
}
Serial.print(buf1[i], HEX);
Serial.print("\t");
}
Serial.println();
}
delay(3000);
}
curious if the LIB has it hardcoded? 8 Bytes
HTH
GL
PJ
I get only, the result is the same:
------------------------------------------------------------------
Get Data From id: 0x7E8
0x10 0x14 0x49 0x02 0x01 0x57 0x30 0x4C