Arduino as connection medium

Hey there,

Im building control system for a servodrive. It’s based on servodrivers

that require connection with the pc.



Normally you take a rj12 (socket in the servodrivers) - rs232 wire, and

since rs232 is widely used in industry it is never a problem. Athough in my

situation there is limited access to devices that accept either rs232 or

rj12. Here comes my question.



Can I use serial connection of Arduino and connect the servodriver via

arduino using rs232 shield and rj12-rs232 wire?



If any clarifications are necessary here hit me back,

Hi Hubert


Please refer to https://www.seeedstudio.com/Grove-RS232-P-2852.html, it turns the uart to rs232 voltage level.


Thanks

best rgds
Bill