Arduino + a 10A relay motor driver board ?

Hi

I just got my Arduino and also a motor driver board and a 10A 450rpm motor.

This is the motor driver board I got:
robokits.co.in/shop/index.php?ma … ucts_id=….

And this is the DC motor I got:
robokits.co.in/shop/index.php?ma … oducts_i….

And also this DC motor from SeeedStudio:
seeedstudio.com/depot/gear-r … p-236.html

I got the motor driver board required for the motor (the first motor requires 9.5A and the driver board allows 10A max per motor). I need such a powerful motor for my project so hence didn’t buy the Arduino’s motor shield.

But now how do I interface this motor driver board with the Arduino?
I’m only connecting one motor of that sort, so I’ll be using only the first two pins on the motor board (pin-1 and pin-2).

Any help on getting this motor driver board working with the Arduino? Huh

P.S: Just received my usb cable, breadboard, harness and motor from SeeedStudio. Thank you guys

–
SingAlong

Sorry but the link does not work… Maybe the supplier of the motor board has more info how to wire it to MCU board. :slight_smile: