Hey guys,
So my my set of Arduino 2WD chassis arrived today and I’ve put it together (will some difficulty! No instructions ).
Take a look here: download.milesburton.com/Arduino … rduino2WD/ (Big fat 56K warn).
If you’d rather see the large pictures in a list see here: download.milesburton.com/Arduino … WD/images/
Impressions so far, not bad for a cheap chassis. The kit could have definitely done with a set of stand-offs for fitting various devious and a manual. My only concern is the wheels aren’t fixed to the motors - my Tamiya wheels have a “hub” which secures the wheel to the motor - a bit of glue should do the job but it’s rather permanent.
Once I’ve hooked up the electronics I’ll update the post.