ArchMAX v1.1

I am the proud new owner of an ArchMAX v1.1. My USB is not providing enough power for the shield.



I have two questions:


  1. The LEDs are flashing, but there is not help on what these mean.


  2. I need to provide external +5v to the board, but I cannot see in the wiki where to apply this on the PCB?



    Any advice most welcome.



    Phil

Hi,



If you are sure the problem related to the power supply, you can power up the device by using the 5v pin.


[attachment=0]Arch_Max_Pinout.png[/attachment]