Arch Pro ethernet init() hang with mbed ethernet library

Hi,

The stadard ethernet examples on mbed hang at init() with the arch pro.
This happens when the library tries to query the MAC address.

extern “C” void mbed_mac_address(char *mac){

mac[0] = 0x00;
mac[1] = 0x02;
mac[2] = 0xF7;
mac[3] = 0xF1;
mac[4] = 0x91;
mac[5] = 0x9F;
};    

This isn’t a question, I just wand to put this out there so that others won’t take the time I did to realize what the issue was.

See the thread on the mbed site:

developer.mbed.org/forum/platfor … ment-26729

Also, I don’t see an mbed section on the forum? Would you rather keep the discussion on the mbed site?

thanks!

Dan