Application note for 2.8 inch TFT Touch Shield v2.0

Hello,
Sadly, my board isn’t supported by the provided library. So I have two options two completely rewrite the provided library, especially for the low-level routines that uses the SPI peripheral or to begin from scratch. Is there an app note available that helps you trough init procedure? (explaining which commands to use, ILItek datasheet is overwhelming and not that user friendly to get started with this display driver…)

Thanks!

which board do you use? Maybe I can help you