Can you please help us deal with the sound problem. We’ve tried all audio options in settings, plugged in headphones, but there is no sound.
Here is the log:
2018-10-24 13:17:04.795 301-805/? E/AudioHardwareTiny: pcm_open(PCM_CARD) failed: cannot open device ‘/dev/snd/pcmC0D0p’: No such file or directory
2018-10-24 13:17:04.807 301-805/? W/StreamHAL: Error from HAL stream in function get_presentation_position: Operation not permitted
2018-10-24 13:17:04.807 301-805/? D/AudioHardwareTiny: start_output_stream
2018-10-24 13:17:04.809 301-805/? D/AudioHardwareTiny: read_snd_card_info buf0 = seeed8micvoicec
2018-10-24 13:17:04.809 301-805/? D/AudioHardwareTiny: read_snd_card_info buf1 = rockchiphdmi
2018-10-24 13:17:04.810 301-805/? D/AudioHardwareTiny: read_snd_card_info buf2 =
2018-10-24 13:17:04.810 301-805/? D/AudioHardwareTiny: now is 3snd card mode
2018-10-24 13:17:04.810 301-805/? D/AudioHardwareTiny: Device : 0x80002
2018-10-24 13:17:04.810 301-805/? D/AudioHardwareTiny: SampleRate : 44100
2018-10-24 13:17:04.810 301-805/? D/AudioHardwareTiny: Channels : 2
2018-10-24 13:17:04.810 301-805/? D/AudioHardwareTiny: Formate : 0
2018-10-24 13:17:04.810 301-805/? D/AudioHardwareTiny: PreiodSize : 512
2018-10-24 13:17:04.810 301-805/? D/alsa_route: route_info->sound_card 0, route_info->devices 0
2018-10-24 13:17:04.811 301-805/? D/alsa_route: route_set_controls() set route 26
2018-10-24 13:17:04.811 301-805/? D/alsa_route: route_set_controls() set route 27
2018-10-24 13:17:04.811 301-805/? D/alsa_route: route_set_controls() set route 24
Hi there,
I went through the adb process and i can record and play correctly. please go through the process again and let us know if any issue. thanks.
<LINK_TEXT text=“http://wiki.seeedstudio.com/ReSpeaker_C … th-android”>http://wiki.seeedstudio.com/ReSpeaker_Core_v2.0/#running-with-android</LINK_TEXT>
Ok, i went through the process, and i’m able to record and play audio (and everything works), but in the android apps there is no sound, how to deal with that?
Hi there,
you can use the tinycap api to record and tinyplay api to play the music. thanks.
And you can give a link to the source code for the image of Android, which is available for download. Just maybe I’ll try to rebuild with the other settings, but I need a driver assembly
Your Android machine is broken and needs to be replaced! :lol: