I got the latest firmware uploaded. Had to use my boarduino with the 328 chip, as my ardiuno with the 168 didn’t work, I think because it is using the same port as the rainbowduino or something?
Anyways, now I have opened compiled mtX. No windows or anything show up but the program runs. If I try and open the uncompiled in the latest version of processing, (I am on OSX 10.5.8 on a dual-G5 mac) and run it from there I get the following error:
File /var/folders/oY/oYdPDQkIFkuRtt1Nqq3zqk+++TI/-Tmp-/build6597409964130728353.tmp/mtXcontrol.java is specified more than once
I am not a total beginner, but nearly so when it comes to java and c++. Any suggestions? I really look forward to trying this out. The rainbowduino has me very excited.
another solution may be to download the source and open it with the Processing IDE. in addition you’ll need the processing launchpad library (rngtng.github.com/rainbowduino) as well.
pls let me know what worked for you, so I can update the docs
cheers