Again asking this from Seeed: why is the XIAO SAMD board, the XIAO ESP32, and the XIAO BLE using nrf52 all put together into one forum?

Again asking this from Seeed: why is the XIAO SAMD board, the XIAO ESP32, and the XIAO BLE with nrf52 all put together into one forum? These are not interchangeable in code and they are only similar in footprint and that they can be used with the Arduino IDE. It is confusing to separate posts that do not mention which board they are talking about.

Hello, thank you for your feedback, we will follow up with corresponding improvements

LOL, No hey won’t…
GL :slight_smile:
PJ