Getting the Something error, suggest you re-plug usb Click to apply message when trying to update the device version on SenseCraft.
Models wont load and come up with the same error.
Have done the boot loader reflash with the I2C connection to an arduino. This did not work until I held the BOOT button down on the Vision AI while connecting the I2C to the Ardunio.
Have tried the 2023.12.19 updated with TERATERM ok. Still wont load models with giving the same error above.
Would like to get a hold of the latest image file if that is possible.
Kind regards