hi,
Seeing the ADK board uses SPI for the USB Host port, is it still compatible with “mega-compatible” ethernet shields?
Yes, it is compitable with “mega-compatible” ethernet shields.
But note, if the Ethernet shield has pin use PB0/SS/D53, you need swap the pin to other IO.
Our Ethernet Shield(use Digital pin 10 as the CS) is compitable with ADK.
seeedstudio.com/depot/wiznet … ?cPath=102
Thanks
Albert
Great, thanks!